CT pin (pin #3 ),This pin can be connected to a capacitor in order to create delay to Reset signals.
Q: what should be the minimum rated voltage of the capacitor?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Eli,
I measured the TL7712A CT pin voltage; it was 3.2V. The internal current source stops charging the capacitor at this voltage.
Regards,
Ron Michallick