Hi Team,
I have a question about the device LP8865Y, or LP8865V.
In the datasheet it is mentioned that the input voltage range is between 4.5 to 65 volts, but the output voltage range is not clear, it is also not clear what would be the maximum number of LEDs in series, and which forward voltage for LED?
Could please make it clear for me?
Can I use 22 LEDs in series? That would be maximum output voltage 82.5V
Do you have such a device that can drive 22 LEDs with Maximum voltage 82.5volt in 350mA as constant current?