This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5001-Q1: LM5001Q1

Part Number: LM5001-Q1

Dear Sir/Madam,

I have selected the part LM5001-Q1 for  SEPIC converter  with input voltage 3.5V to 15V  and output voltage of 12V . When i am selecting the output current of 230mA on TI work Bench it says "Design update failed. Can't find suitable FET for the design. Try reducing load current This device has CC enabled but there is no circuit calculator found."

Please tell the solution