Other Parts Discussed in Thread: BQ24076
Hi,
I've just noticed that when there is no battery connected to BQ24073 and CE pin is low (charging enabled) then output voltage is around expected 4.4V. But as soon as I pull the CE pin high (charging disabled), the output voltage drops to around 3.4V, which is enough to power my LDOs but a bit low to operate cellular module. I was expecting BQ24073 to continue to regulate output voltage to 4.4V. Am I missing something? Please can anybody point me to the relevant part of the datasheet that would describe this behaviour?
It's not caused by current limit because I measure single milliamps when this happens.
Thanks