Other Parts Discussed in Thread: BQ28Z610
Hi,
I found some inconsistencies in the selection of balancing resistors. In the BQ28Z610-R1 (SLUSE07A) datasheet, page 19, paragraph 8.3.13, balancing resistors with a value between 100ohm and 1Kohm are recommended. In the same datasheet the example diagram shows RVC2 = 5 ohm. In the Technical Reference (SLUUC81) on page 42, Cell Balancing Setup, RVC2=105ohm is calculated. What is the correct resistor to put in series with VC2? 5ohm or 105ohm?
Regard,
Paolo Colombo