Hi
The customer test with BQ40Z50-R1, the problem is after discharging from 68% to 8% and manually stopping it, let it sit for a while and the SOC will rise back to 9%.
The CHEM ID is selected and full learning.
Attached the gg file and log data.
CN070-AC放电到SOC4%后关输出再按点烟口按键SOC跳变为7%.csvCN070-BMS模拟AC300放电-SOC4%跳7%.logCN070.gg.csv
Please help check it.
Thanks
Star