Hi TIer
My customer uses this adjustable version of the LDO to output a voltage of 1.2V. However, due to resistance accuracy issues, the setting voltage of the voltage dividing resistor may be around 1.15V~1.18V. The customer wants to know whether there are hidden dangers and risks in such an output?
Also I saw that our internal reference voltage is 1.1834, what happens when our external setting is less than the reference voltage?
I think that if the output voltage continues to be lower than the reference voltage, the pass MOSFET will continue to increase the degree of conduction, and eventually the output voltage will stabilize to the reference voltage of 1.1834V without the output being lower than the reference voltage. Is my understanding correct?