Other Parts Discussed in Thread: BQ24316
Attached to this posting is a schematic of a single cell Li-Ion charger. The charger contains BQ24090 supervised by BQ24316.
Why did the circuit designer include a 555 timer that zeroes out the TS pin of the BQ24090 for 2 seconds at the time the battery is inserted into the charger?
Battery presence detection is accomplished using pin #6 (BATTERYPRESENT) of battery connector P1. Internal to the battery module its pin #6 is grounded to the battery's minus pin.
When the battery module is inserted into the charger the negative-going pulse on BATTERYPRESENT triggers the 555 timer and grounds the BQ24090's TS pin. Why?
18650 Smart Cell Charger.pdf