This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMQ66410: LMQ66410, min operating voltage

Part Number: LMQ66410

Hello,

The FB voltage is 1V. Is it possible to regulate the output voltage to 1V?

Conditions : VIN : 5 to 17V, Iout max 0.4A, external clk 750KHz (ton min max = 75ns)

Do you have any other reference to suggest? The main criteria is efficiency.

Regards,

Arnaud