Other Parts Discussed in Thread: LMQ644A2-Q1, LM25148, LM5145
I need a buck converter than can accept input voltages in the range of 9V to 36V
Continues current 8A and peak current 15A
Output voltage = 7.4 and 8.4V
It would be great if it is available on Webench Tool or some reference design.
Thanks