This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5907-Q1: There is a power-on overshoot

Part Number: LP5907-Q1

Hi,

I have clients who use this LDO to design circuits with undercharge phenomena.

The front-end DCDC is 12V to 5V. There is no overshoot during power-on. Only LDO output overshoot occurs.

The schematic design and waveform test are shown below. Please help to find out the reason.
Confirm that LP5907QMFX-3.3Q1 is used, and the model in the schematic diagram is not modified.
Thank you!