This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40425: How to use TPS40425 for one phase configuration in tool of DC/DC Power Designs

Part Number: TPS40425

Hi Teams,
In WEBENCH@ POWER DESIGNER, I select TPS40425 (buck controller with SPS) in DC/DC Power Designs. TPS40425 is a two phase controller combined with two SPS (smart power stage). In DC/DC Power Designs, TPS40425 is always designed to two phase operation no matter what's designed output current. How can I change the two phase to one phase operation in this tool? Besides, I can't select SPS (M1 and M2) alternative part number in bill of material.