Hi,
in our application we are using the TPS78450 as a second stage regulator, powered from a DC-DC converter as shown in Figure 8-8 of the datasheet.
I would like to use a reverse current protection diode across TPS784, from the output to the input, like it is mentioned in section 8.1.7 and Figure 8-5 of the datasheet.
There is however the question about what diode should be selected and what criteria it should fulfill.
- Why is it mentioned that a Schottky diode with low forward drop voltage should be selected? Why low forward drop is important?
- Then, how much forward current should the diode withstand?
- Are there any other important parameter to consider?