Other Parts Discussed in Thread: TPS62A02
Dear Team,
Does TLV62569 can meet this spec as below? Thanks a lot.
if not, please suggest suitable solution. Thanks.
Many Thanks,
Jimmy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Jimmy,
Thank you for reaching out,
If it's a new project i would recommend TPS62A02, which is our value line hero device. It has lower feedback tolerance across the temperature compared to TLV62569.
Please see the comparison below between TLV62569 & TPS62A02.
Please provide me your typical load current so that i can check the output voltage ripple requirements. And also please make this question internal.
Thank you & regards,
Moheddin.
Hi Moheddin.
Thanks for your great support.
For 1.9V Current consumption is 0.595A. Thanks
Jimmy
Hello Jimmy,
Thanks for providing the operating conditions.
With Vin = 3.3V, Vout = 1.9V, Iout=595mA, the ripple is lesser than 10mV, with just a 22uF Cout.
Please note that these measurements are performed by using TPS62A02EVM-197 Evaluation board | TI.com
Thank you & regards,
Moheddin.
Hello Jimmy
If you don't have any further questions can you please close the thread by clicking on Resolved.
Thank you & regards,
Moheddin.