Other Parts Discussed in Thread: BQ24105-Q1, BQ25171-Q1, LM51231-Q1
Dear Team,
E-CALL has been evaluated to operate in an environment of -40 to 85 degrees Celsius.
We will use nickel metal hydride battery pack. I hope the charging current can be edited.
Then there are car regulations for charging IC applications in 12V systems
If Vmax. can reach 36V, please recommend it.
Also, I would like to ask which IC is used to convert mainstream 12V system DC/DC to 5V?
The maximum output current is first evaluated at 3A.
Do you have any recommendations for Boost IC (NiMH battery voltage should be at least 3 strings = 3-3.6V)
The voltage will rise to about 9V and the output current is estimated to be about 4A.
Many Thanks,
Jimmy