This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28065: How to Dynamic adjust the R_TSET for UCC28065

Part Number: UCC28065


Hi, Team

My customer use our UCC28065 in their PFC power module, they  prefer Dynamic adjust the R_TSET  for UCC28065, the detail is as below:

As we know, the R_TSET value is control the Ton time( or max ton time) of the UCC28065. the Max_Ton_time limit the max output power.

that means we can change the R_TSET for different output power requirement.

So customer prefer to adjust the R_TSET value for different output power.

For example, if Vin_ac is high, increase the output power by increasing the Ton time.  and if Vin_ac is low, decrease the output power by lower the Ton time. So they prefer use R_TSET value for different Vin_AC to control the Ton.

Base on their requirement, we suggested them using MCU GPIO pin to set deference R_TSET. (GPIO control a Mosfet On/off, and the Mosfet control the R_TSET), just like below:

For our suggestions, customer think it’s OK. But they feedback that add 1 more Mosfet can only add one R_TSET step.

They prefer add more steps base on their system’s requirement. They prefer TI to check whether they can use MCU PWM to get more step, see as below: (PWM signal output from MCU, and use RC filter to get a DC value to TSET pin.

 

1, Could u help to check whether we can use PWM+ RC filter to adjust the Ton time?

2, if not, Do u have any others suggestions base on customer’s requirement?

Thanks.

GW