This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62842EVM-103: When outputting with load, the input voltage fluctuates

Part Number: TPS62842EVM-103

Test conditions: Input 6V, output 3.6V, with a load current of 15mA

Result: The input voltage fluctuates; Under no-load conditions, the input voltage is stable

Could you please help determine the reason? Looking forward to your reply. Thank you