This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS566238: TPS566238PRQFR Design Review needed

Part Number: TPS566238

Hi,

Need design review of the below design:

This circuit is used to power a LTE modem, where there is huge inrush current during startup, as high as 3A, need to make sure this circuit can handle it.

Also the input voltage can vary between 3.3V to 4.2V.

We are trying to send this board to FAB in the next 2 days. So a review would really help.