Hi team,
Do we have TPS61252 TINA file? The customer want to use this file to simulate frequency domain simulation? Or could you help simulate when Vin is 3.6V and Vout is 3.3V ,Io is 1.4A
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Do we have TPS61252 TINA file? The customer want to use this file to simulate frequency domain simulation? Or could you help simulate when Vin is 3.6V and Vout is 3.3V ,Io is 1.4A
Hi Hale,
We don't have this file for TPS61252. But TPS61252 is hard to output 1.4A under 3.3-3.6V condition. Please view datasheet 10.3.2 to calculate the output capability. If you're changing devices, tell me the feature you requires and I'll recommend another IC.
Best Regards,
Travis