This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2121: or similar with automotive grade component?

Part Number: TPS2121
Other Parts Discussed in Thread: TPS2115A-Q1

Automotive Grade TPS2121?

Any equivalent to the TPS2121 or similar automotive grade component?
other than TPS2115A-Q1, I need help connecting 2 power supplies (Master-slave), one 12V (master) and another 16V backup (slave) with a current of 2A to 3A

Best Regards.