Hi Experts,
We assembled three pieces of boards using TPS22992, and we have found one of designated TPS22992 corrupted on all of the three boards. Although we use two TPS22992's on the board, one of them was fine. The corrupted ones are used for simple 5V line ON/OFF switch. And those failed boards have been working fine after replacing TPS22992. All of TPS22992's, corrupted ones, fine ones and replaced ones, are exact same batch from one reel.
I attach the circuit diagram of the corrupted one, and damaged photo of the worst damaged one. Regarding other two board, there are no visible damage, but don't work. It looks burnt so the direct cause might be electrical stress rather than physical stress.
I have been thinking the cause of this issue, however there is no idea. Does anyone have any idea? Even any possibilities would be help for me.
circuit_diagram_TPS22992.pdfDamage_photo.xlsx
Regards,
Tetsuya