Hi,
My customer is doing evaluation with LMR33620 with two similar schematics and PCBs.
For the one w/o EMI filter on input 33620-62850, the current will directly go beyond the current limit of the digital power supply (set up as 1A) when starting up with empty load.
However, for the 33620-87702 with EMI filter, the current seems normal and start successfully with empty load.
The schematics are as attached, does an EMI filter a must for the LMR33620? What might be the reason cause the unexpected high current during start up with empty load?
33620-62850.pdf33620-87702.pdf
BR,
Manu