This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53219: Could change the OVP time

Part Number: TPS53219

Dear Expert

Can the internal OVP time of the IC be extended for a longer period of 1uS when testing for electrostatic discharge in the safety category .

  •  

    No, the internal OVP timing is fixed, there is no way to extend it.

    Since the OVP responds to the voltage on the FB pin, you could add a capacitor from FB to GND to slow down the dV/dt of the FB pin and delay the pin reaching the OVP threshold.

    If you are using RCC injection to allow D-CAP control to work with low ESR output capacitors, you could consider reducing the value of the DC blocking injection capacitor to reduce the high-frequency injection of Vout transients into the FB pin.