This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24171: BQ24171 battery detect flow

Part Number: BQ24171

Hi

The customer design with BQ24171 to charge the 2 cells. They follow the datasheet 9.3.15 to do the battery detect test.

It was found that at the beginning of charging, charging stopped after maintaining a 100mA charging current for about 500ms, and the charging stop time was also about 500ms. During the period of stopping charging, the state changes from H to L. Then increase the charging current.

Attached the waveform.

Yellow: battery pack voltage

Blue: SW of charging IC

Red: charging current

Green: State of charging IC

Does it comply with the process in 9.3.15? The 125mA charging current is the red box part in flow? The 500ms to stop charging is Is it the switching time to start the official charging?

Please help check it.

Thanks

Star