This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC25660: UCC25660 Low Voltage Application Efficiency Performance

Part Number: UCC25660

Hi, 

I am planning to use UCC25660 IC in low voltage input application. Where the specifications are Vin=48V; Vout=24V/30A.

In the datasheet the efficiency curve is given for HV input conditions. Does the efficiency similar to the given curve in our specifications? If not what is the approximate efficiency levels? Is there a limit to reach 97% efficiency levels with this IC?

Thanks for the help.