Hi,
The input voltage is 3.3V and trying to generate a 3V reference voltage for MC Vref.
Our 3.3V voltage range can vary +-5% that is from 3.135V to 3.465V.
Is it possible to use LM4040BIM3X-3.0/NOPB part for our application?
Regards
Vishnu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
The input voltage is 3.3V and trying to generate a 3V reference voltage for MC Vref.
Our 3.3V voltage range can vary +-5% that is from 3.135V to 3.465V.
Is it possible to use LM4040BIM3X-3.0/NOPB part for our application?
Regards
Vishnu
Hello Vishnu,
The LM4040BIM3X-3.0/NOPB will work in your application depending on the load current required. The LM4040BIM3X-3.0/NOPB requires a minimum operating current of Iq=67uA and has a max output current of 15mA. Rs must be selected so that (3.135V-3V)/Rs >= 67uA + IL and (3.465V-3V)/Rs =< 15mA. This gives a minimum resistance value of 31 ohms which means when Vs = 3.135V the maximum load current possible is 4.28mA with a 31 ohm input resistor. If less load current is needed, a larger resistor can be used up to 2k ohms when IL=0.
Best,
Walter