Other Parts Discussed in Thread: LM5123-Q1
Hello TI,
I am doing a booster design for a customer using the LM5123-Q1, and I have a couple of questions:
1) In the datasheet, it says: "For stability reasons, the VREF capacitor (CVREF) should be between 330 pF and 1 nF. 470 pF is recommended."
In the application note, on "Figure 1-1. Typical Application", a 470nF capacitor is placed.
Can i assumme that the datasheet is correct?
2) What is your recommendations with regards to added an aditional gate resistor to reduce ringing?
3) Since it is a 5V FET driver, I am planning to design with GaNFETs. GaNFET generally have a gate voltage limit of -4V to 6V, so I do not see any reason why it would not work. What is your opinion?
I am looking at using EPC2067.