Is the TLV75901PDRVR a suitable replacement for the R1173H001B-T1-FE? If not, is there a different alternative I should recommend?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is the TLV75901PDRVR a suitable replacement for the R1173H001B-T1-FE? If not, is there a different alternative I should recommend?
Hi Abigail,
TLV75901PDRVR is the closest specs-wise. Quick comparison below:
TLV75901PDRVR | R1173H001B-T1-FE | |
Iout(Max)(A) | 1 | 1 |
Vin(Max)(V) | 6 | 6 |
Vin(Min)(V) | 1.5 | 1.4 |
Vout(Max)(V) | 5.5 | 5 |
Vout(Min)(V) | 0.55 | 0.8 |
Fixed output options(V) | ADJ | ADJ |
PSRR @ 100 KHz(dB) |
45 | 45 |
Noise(uVrms) | 53 | 30 |
Accuracy(%) | 1 | 2 |
Dropout voltage (Vdo)(Typ)(mV) |
190 | 180 |
Iq(Typ) (mA) |
0.025 | 0.06 |
Output capacitor type | Ceramic | Ceramic |
Thermal resistance θJA(°C/W) |
80 | 110 |
Operating temperature range(C) |
-40 to 125 | -40 to 85 |
Package size: mm2 | 4 mm2: 2 x 2 (WSON|6) | 19.57 mm2: 4.5 x 4.35 (SOT-89|5) |
Regards,
Andres