Hello,
We have recently built boards utilizing the TPSM63603 as a 5v and 12v regulator from 24V. Of the initial 10 boards we built, the 5v TPSM63603 has failed on two. In both cases, Vin and Vout are shorted on the chip itself, shorting out the entire board. Is there any protection logic recommended for these modules during power on? We used the data sheet example 8.2.1 for the 5V implementation, excluding the RENT RENB resistors. Vin is connected directly to En/SYNC. Are there any troubleshooting recommendations for the part itself?
Thanks