Hello,
I'm considering TLC5941-Q1.
The circuit I created has the following problem:
LED24 and LED27 have different brightness, with LED24 being brighter and LED27 being darker.
When observing the voltage of OUT10 (LED24) and 11 (LED27), the following waveform was observed.
The difference in the brightness of the LED seems to be the difference in the voltage level when the LED is lit.
What settings should I make to make the LED dimly light like OUT11 (LED27)?
Best regards,