Good day,
I am testing the chip TPS22950CDDCR with Ilim resitor set to 22k. I am expected the device to drop the voltage when current exceed 50-60mA. This seem to happen only if I set my load switch to current higher than 60mA and then power and enable device. When the device is already enabled and powered and I slowly increase the load the device. Over current protection never activates and I can go to 100mA and above and output voltage is still the same at 3.3V.
From my understanding the over current protection should limit the current and then drop the output voltage. Does does note seem to happen.
Please explain if I am misunderstanding how the device functions
Kind Regards
Andre