This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65265: XC9263 Cross

Part Number: TPS65265
Other Parts Discussed in Thread: TPS563252, TPS563240

Hi team,

I have a customer who needs an alternate for the XC9263A75CMR-G. The footprint would need to be around the same, which is in a SOT-25 and a 5-pin configuration of Vin, Enable Soft Start, FB, GND, Switching output.

Input voltage range: 3-18V

Output Current: 500mA

1.2MHz SW Freq

Type A: Integral Latch Method

Let me know if you find anything! Thanks in advance

Marco

TOSL_S_A0012984223_1-2575115.pdf

  • Just to add additional context, the pinout is the most important piece here. A 6-pin part with the same configuration will still do the trick. This design is already in production and trying to avoid a board spin

  • Hi Macro,

    We do not have such part of SOT235 pkg at present. For TI SOT236 part, TPS563240 would be similar with this competitor but not P2P and No SS&PG function either. For SOT563 part, TPS563252 would be similar with competitor but not P2P either.

    Could you please help to persuade customer to evaluate TPS563252?

    BRs

    Zixu