This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello expert,
We are using UCC28600aux_secondary.pdf for aux power supply 24V output. Input is from 200VDC to 1000VDC. We've modified REF_62W_FLY_1700V_SIC to have only single 24 V output. But the device shuts periodically with no or light load. Can you please look into the design (attached) and verify it?
Regards,
Jitendra
Hi Jitendra,
Thank you for the query on UCC28600.
I think the overall schematic looks fine.
I have attached the calculator also where you might need to slightly adjust the Rovp1 and Rovp2 resistors.
Ensure that the capacitor on CS and FB pin are as close as possible to the IC pins.
The snubber circuit can be tuned further as I think it could be to OVP. Consider adding a resistor in series D12 (around 30ohms) and also in series with D13 (10-20 ohms) as this can help with damping some energy at turn off time of the FET.
Also the snubber resistor could be increased to 100k with appropriately tuning the snubber cap to 1-4.7nF to damp out the high frequency ringing potentially truggering this shutdown.
Regards,
Harish
Hi Harish,
Thanks for looking at it.
Adjusting Rovp1 and Rovp2 resulted in continuous operation. We will review the snubber as well.
Regards,
Jitendra