This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD88539ND: Spice Model CSD88539NDT

Part Number: CSD88539ND

HI Folks,

I am working on a Cadence PsPice simulation examining the Vds voltage drop at 1A and other design  parameters, I am looking for a spice model to incorporate in my design. After looking online I do not see a model for this part and my simulator does not have one. Could TI post a model for this N channel MOSFET (CSD88539NDT) . Thanks for your time in advance.

  • Hello BOb Wagner,

    Thanks for your interest in TI FETs. There is an unencrypted PSpice model available in the CSD88539ND product folder on the TI website. Click on Design & development and you will find the model under the Design tools & simulation tab. You can also download it at the link below.

    https://www.ti.com/lit/zip/slpm110

    Best Regards,

    John Wallace

    TI FET Applications

  • HI John, Thanks so much for the help in getting the model. One thing I notice when simulating is I am getting much more voltage drop from Drain to source than expected. I am applying a Vgs of 10Vdc and a cirrent Id of 1A. Based on the data sheet, I was expecting a small Vds of about 0.02V. I am getting about 2V. I am looking at Fig. 4,2 in the data sheet of Ids vs Vds, which shows a small Vds at these conditions. Am I miss understanding the data sheet? Thanks again for your help in advance. 

  • HI John,

    I figured out the problem, the model is fine. My load was not on the correct side of the FET, so the Fet drive was not as high as I originally thought. Thanks for your help and patience.