Other Parts Discussed in Thread: BQ24070
Hi!
I'm using the BQ24070EVM board to validate our design.
At the moment the EVM is unmodified except for the addition of 2X 10uF caps from BAT+ to BAT-. These 2 are in parallel with the 10uF on the board, bringing
the total capacitance to ground equal to 30uF.
The battery is a single 18650 Li-Ion cell.
Instead of a wall adapter, the chip is powered by a lab supply set to 5V and the current limit is set to 1.25A.
JMP1 is set to 0.5
JMP2 is set to HI
JMP3 is set to EN
R_DPPM is set to 35.7K (TP1)
R_TMR is set to 50K (TP2)
All LED jumpers are installed.
There is a 20 ohm resistor connected from OUT to GND.
VIN is 5V
In "standard" operation the charging worked fine. It charged a drained battery nicely at a constant 1A until it tapered off and terminated the charging at a 100ma threshold.
Then I tried a few twists.
Partially charged battery. (Still taking 200ma of charging current).
[1] Remove the 5V input. Leave the battery in place. After a period of time, start up the 5V supply again.
All good.
The battery supplies the load current and when the 5V is powered up again, the charging resumes. (STAT1 LED on, STAT2 LED off).
[2] Starting with the 5V supply off and the battery removed. Insert the battery, and after a period of time, start up the 5V.
All good.
The battery is inserted, it is supplying the load current.
Then the 5V is turned on. Charging starts and the 5V supply is feeding the load current.
[3] Start with the 5V connected and the battery installed...Battery removal and replacement....(This test is to emulate a battery change in the field while the unit is powered on by the 5V).
Not working as expected.
Starts with normal charging operation as the 5V is on and the battery is installed.
Then the battery is removed.The 5V is always connected.
With the battery removed, the 5V supply is feeding the load current, as expected.
When the battery is reinstalled, STAT1 LED is off, STAT2 LED is on. No charging.
In order to get the charging to start up again (STAT1 LED on, STAT2 LED off), the 5V supply has to be turned off and on.
What do you think is happening is this case? Suggestions?
[4] Powering up the 5V with no battery installed.
Not working as desired.
Comes up in one of short circuit modes I think. Consuming 10ma from the 5V rail.
When the battery is connected, charging does not start. Still consuming 10mA.
What do you think is happening is this case? Suggestions?
Thanks and Best Regards
Jerry Molnar