Other Parts Discussed in Thread: UCC21750
Hi Team,
We are using the part number ISO5852-EP. Followings are the technical question for the same part.
1. As per data sheet (VIT+UVLO) is typ-12V , Max-13V and (VIT-UVLO) is typ-9.5V to max-11V. so, question is if we are using the VCC2 supply 12V with +/- 0.2%. will it be ok to use it ? Please give your suggestion and if you have any more technical details UVLO typical and worst case please share it with us.
2. is there any other pin drop replacement with similar kind of Gate driver series with lower UVLO 8-9V ( Note that we do have 12V +/- 0.2% power supply available in PCB). Please suggest any part or series.
Regards,
Hardik