I am going to test current limit of TPS568215, could you pls share OCL test result/waveform of TPS568215 EVM to me?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Please check attached waveforms. One is zoomed in waveform right after OCP is triggered which triggers the UVP delay and then the IC shuts down. Since I continue with the OCP condition, IC restarts after a hiccup time of 7 soft-start cycles. OCP limit is ~7A since ILIM1 is selected.
OCP trigger + shutdown after UVP delay
OCP continued - IC restarts after hiccup time of 7 soft-start cycles and continues till OCP condition exists as below
Thanks,
Amod