Other Parts Discussed in Thread: TPS2116
Hi,
we are using LM66200DRLR to switch between 5v USB input Vin1 and battery input 3V-4.2V VIn2.
when there is switching(system is running on battery and USB is connected OR when system is running on USB and USB is disconnected) between the two there is a dip which results in our system reset.
- what can be the solution to stop the dip?
- do we have a part which resolves this issue with continuous power output management in same package