Hi team,
This is FAE Jayden, my customers are using TPS62875QWRZVRQ1 to produce 0.55 v at 16A current, ripple = 40 mV, > 85% efficiency in 800G optical module. Input voltage is 3.125-3.46V. The inductors provided by the Power Designer are too big for our application.
Can you please provide alternative in small footprint? Can they use similar or same as inductor XEL4020-800MEC? I found a similar XEL4030-101ME is recommended in datasheet.
If so, what is the minimum capacitance to have a stable design when using XEL4020-800MEC? can the min recommended Cout 47uF keep the design stable? Thanks.
Brs
Jayden