This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62875-Q1: alternative inductor recommended.

Part Number: TPS62875-Q1

Hi team,

This is FAE Jayden, my customers are using TPS62875QWRZVRQ1 to produce 0.55 v at 16A current, ripple = 40 mV, > 85% efficiency in 800G optical module. Input voltage is 3.125-3.46V. The inductors provided by the Power Designer are too big for our application.

Can you please provide alternative in small footprint? Can they use similar or same as inductor XEL4020-800MEC? I found a similar XEL4030-101ME is recommended in datasheet.

If so, what is the minimum capacitance to have a stable design when using XEL4020-800MEC?  can the min recommended Cout 47uF keep the design stable? Thanks.

Brs

Jayden