This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC21530: Programmable Dead time with shoot through protection

Part Number: UCC21530

Hello,

1. We are looking for part with Dead time feature of around 400nsec, Shoot through protection.

What is the max dead time setting can be done with UCC21530 IC? 

Some datasheets we can see dead time with respect to resistor values at DT pin. 

We can see 20K resistor value only. 

2. Is there any part with dead time of around 400nsec and shoot through protection integrated?

Supply voltage 12V

Regards,

Sudharshana