Other Parts Discussed in Thread: SN6501, UCC21551
I want to use UCC5350MC to drive the MOS transistor in the BUCK circuit, and I would like to ask:
(1) How do I connect the VEE pins on the secondary side of the chip? Can it be directly connected to the S-level MOSFET? (Because generally speaking, VEE needs to be grounded to a power source. If connected to an S-level, the VEE becomes a floating ground.)
(2) If possible, is it necessary to connect a resistor in series between S and VEE to avoid the impact of the switch on the driver chip.
(3) Is there a recommended application circuit diagram?