Other Parts Discussed in Thread: LM51772, LM5171, LM5117, LM5177, LM5171-Q1, BQ77PL900, BQ78PL114, LM5171EVM-BIDIR
I need to design a board that can connect 14 of these TPS55288-Q1 devices to replace the Vicor VTMs, as we need to step up the voltage from 3 volts to 22 volts. This tricks the grid-forming enphase microinverter into discharging the High-Temp Sodium Ion Battery Cell, which can charge and discharge at 85°C and -70°C. We also need to step down the solar module voltage, which ranges from 24-36 volts, to charge the 3-volt battery. We would program the device to charge the battery early in the morning when the voltage is low and discharge it when the sun goes down. We want the electronics to last 20 years like a solar module and battery cell.