Hi,
Customers ask questions.
The red rectangular circuit is the Secondary Flyback output.
However, the physical location is in the input.
The current circuit has a 6.7V output.
The customer would like to ask if the feedback Ref voltage can be received to the VCC so that the output except diode Vf is 5V.
Currently, it receives 6.7V, and 6.2V excluding Vf is inputted as LDO and it is 5V.
In order to remove LDO and generate 5V output directly, I think I need to get 5V output to FB.