Other Parts Discussed in Thread: TPS2116
Hi all,
As shown on the right, Ch2 is Vout & Ch4 is ST. The voltage droop reaches to 2.75V from 3.3V supplies. It should be noted that Both Vin1 & Vin2 are 3.3v. The load used is the on-board 10ohm resistor. Furthermore, we've also used constant-resistance load varying from 50-10 ohms. The issue still persists.
Could you please advise? We've tested for all three priority mode voltages (1.8, 3.3, 5). They all show 15%-20% droop.
Yours,
Ibrahim.