This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, I am using the TPS23734 and switching mosfet is heating when connect the load 50mA.POE-TPS23734RMTR.pdf
Hi Sandeep,
Thanks for reaching out.
I am wondering if you want to use a active clamping forward structure. If so, please refer PMP23278 reference design for the secondary side and the transformer.
https://www.ti.com/tool/PMP23278
Best regards,
Diang
Hi Diang,
I have add the secondary circuit which is used in PMP23278 reference design and on the power IC TPS23734 is Instantly not work I remove the secondary circuit and change the IC after that we have added a diode (40V/3Amps) to transformer output and then connect the secondary circuit the circuit is working fine but IC is heating without load.
Both reference Images is attached.
Regards,
Sandeep Kumar
Hi Sandeep,
Thanks for your information.
I think the transformer you selected (PA2467NL) is for flyback converter instead of forward converter. I think the transformer may cause the failure when you use PMP23278's secondary side.
If you want to use the forward converter, I would recommend you to change the transformer as well.
Best regards,
Diang