Other Parts Discussed in Thread: PMP10979,
Hi,
I'm searching for a very high efficiency DC-DC buck converter for a new design, with the following parameters:
Vin = 12V or 24V
Vout = 2.4V,nom
I,out,nom=25A
I,out,max=40A
Searching TI parts, I notice the LM25119 has a reference design, PMP10979 with a purported 98% efficiency (condition dependent, see chart below taken from PMP10979 Test Results):
However, when I used WeBench for my design, the tool tells me to expect a max efficiency of 92.4% (I used my own design requirements as stated above).
Here are some questions:
(1) Why is there such as difference in efficiency between these test results and the WeBench?
(2) Is more data available for the LM25119, for example an efficiency graph for a single device (I recognize the PMP10979 is 4-phase with 2 devices, instead of a 2-phase 1 device design)?
(3) Is there a different VR that may be more efficient and more suitable for my design?
Thanks,
Tom