This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello TI team,
I'm about to use: BQ76942, Communications Interface: I2C, REG1 LDO default: disabled.
Not intend to use internal LDO, REG1 and REG2. Run BQ76942 in fully autonomous mode, no external MCU.
REGIN and BREG connected to VSS.
REG1: floating
REG2: floating.
Calibration and OTP programming will be done by using external equipment. Pull-up for I2C will be on placed in
external equipment. Attach simplified block diagram.
Cells will be assembly after calibration and OTP programming.
Question 1: Is it possible to communicate BQ76942 according to attached block diagram? Guess REG18 is used for internal logic.
Question 2: Once calibration and OTP programming is done, pull-up on SDA and SCL is left floating, is that okay?
Question 2.1: If floating is not okay, how should SDA and SCL be handled since I can't have pull-up to REG1?
Regards,
Andreas
Hello Andreas,
It is perfectly okay to use an external regulator for the pull-ups, you do not need to use REG1/REG2 with our I2C.
Question 1: Is it possible to communicate BQ76942 according to attached block diagram? Guess REG18 is used for internal logic.
Yes, this looks okay to me . 3.3-V pull-up should be more than okay. Pull-up resistors may be better to be slightly larger, we use 10-kOhm pull-ups in our EVM.
Question 2: Once calibration and OTP programming is done, pull-up on SDA and SCL is left floating, is that okay?
Yes, that is okay if you are not interfacing with a MCU. Keep in mind that during OTP, the BAT and VC10 voltages need to be ~11-V or so.
Question 2.1: If floating is not okay, how should SDA and SCL be handled since I can't have pull-up to REG1?
See answer above. These can be left floating.
Let me know if there are any additional questions!
Best Regards,
Luis Hernandez Salomon
Hello Luis, thank you for fast response. Very much appreciated!
Have a nice day!
BR,
Andreas