Dear Expert
Could you please provide the following data for IC model BQ2022ADBZR? Thank you
1. What is the actual maximum withstand voltage of the IC? If the IC is damaged during testing, it is necessary to provide more than 10PCS of data.
2. According to the following circuit, connect SN to DC+, OP - to ground, and increase the voltage of SN from 3.3V to confirm the voltage when the IC is damaged. Record 5PCS..
3. SN connected to 19.5V, what resistance value can R28 use to ensure that the IC is not damaged.