This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24074: Charger does not stop charging when the terminate current is reached

Part Number: BQ24074

Hello, I am having a big headache with a charger circuit that I have design for my application. The circuit is presented by the circuit below.

The battery is reaching 4.4V and the charging current goes as low as 30mA (or even less) without stopping the charge.

I tried to:

  • Change Rterm to 10k;
  • Remove Rterm.
  • Connect TMR to GND
  • Short the current sensor and the choke to reduce the impedance.
  • Add a 4.7uF in parallel with C2 (close to the BQ).

Any advice is much appreciated.